Offshore wind farms are gaining momentum as a vital source of renewable energy. As countries strive to reduce their reliance on fossil fuels and lower their carbon emissions, offshore wind farms offer an excellent opportunity to generate significant amounts of electricity using the power of wind over the open ocean. However, developing offshore wind farms is a complex and challenging process that involves significant technological, logistical, and financial considerations. From initial site selection to project construction and ongoing operation and maintenance, starting an offshore wind farm business requires careful planning and execution.
To support companies in the offshore wind industry, Panduit has expanded its portfolio with the acquisition of Subsea Cable and Pipe Protection Product Portfolio from DongWon EN-Tec Co., Ltd. With this acquisition, Panduit can now offer a more comprehensive range of high-quality industrial products to its Asia-Pacific customers, including power cable and fiber optic subsea cable protection against hazardous conditions. By diversifying its customer base and expanding into offshore alternative energy and global communications bandwidth markets, Panduit is at the forefront of megatrends in the industry.


URAPROTECT™, developed by Panduit, is a cost-effective and efficient solution for protecting subsea pipes and cables from abrasions and impacts during installation and operation. It is designed as a protective "sleeving" that can be installed on the pipe or cable as it is laid or offloaded. This helps to minimize the need for additional vessels or equipment and reduces project costs.
Bend Stiffener is used to limit bending stress and excessive curvature on cables and umbilicals at the point of connection to a rigid structure. Panduit's Bend Stiffener systems can be used in static or dynamic applications and are designed to add local stiffness to the cable or umbilical. The system typically incorporates integral steelwork required to interface with the client's connecting structures.
Bend restrictors are typically used in static applications where there is a possibility of over bending or damage to the pipe structure. They can be used onshore, offshore or subsea and are often used to support flexible pipes over free spans. Some common applications include wellhead connections, PLET connections, J-tube exits, rigid pipe crossovers, and over subsea buoys at the interface between flexible and rigid structures.
Panduit J-Tube Seals are designed to provide a reliable and effective solution for sealing the interface between the inside of a J-Tube and the riser. The seals help prevent the loss of water containing a corrosion inhibitor that is introduced into the J-Tube void space. They are designed to be robust and effective in harsh environments, such as those found in offshore and subsea operations..

Image credit: Doosan