Panduit Cat6A Vari-Matrix HD: the world's smallest Cat6A UTP cable supporting 1-10GbE and PoE++, with superior signal protection.

The year 2023 presents a dynamic and fascinating landscape for the network signal industry. Manufacturers are pushing for new innovations and competing on multiple fronts, including advancements in Ethernet speed, improved support for IoT devices, and increased focus on sustainability.
As a prominent technology provider of network infrastructure systems, Panduit has unveiled its latest product - the Panduit Cat6A Vari-Matrix HD, the world's smallest Cat6A UTP cable. This product features several state-of-the-art technologies that surpass the standard Cat6A, making it a compelling solution to consider for designing indoor cable systems. Hence, it is worth exploring the exciting capabilities that this product has to offer.
The Panduit Cat6A Vari-Matrix HD is the world's smallest Cat6A UTP cable.
Panduit highlighted the Cat6A Vari-Matrix HD cable as the world's smallest Cat6A UTP cable during its launch. Featuring 23 AWG copper and incorporating various Panduit innovations, it offers a cost-effective, flexible, and eco-friendly option for network cabling installation. Additionally, the Cat6A Vari-Matrix HD delivers superior performance beyond the standard Cat6A.

Here are some interesting features of the Panduit Cat6A Vari-Matrix HD cable:-
- Panduit Cat6A Vari-Matrix HD offers a cost-effective solution for upgrades or new installations.
With a center conductor diameter of just 6.2 millimetres, the Panduit Cat6A Vari-Matrix HD cable is recognized as the world's smallest 23 AWG Cat 6A UTP cable. Yet, it can provide reliable signal services that support Ethernet speeds ranging from 1-10 GbE. For businesses planning to upgrade from Cat6 to Cat6A, the same cable management equipment can be reused in most cases. Nevertheless, using Cat6A-compatible cable management equipment can increase the cable run capacity by up to 25%, which enhances the value of their investment in upgrading or installing new cables.
- Comes with Vari-MaTriX technology, reducing signal interference and surpassing Cat6A standards.
The Vari-MaTriX technology used in the Panduit Cat6A Vari-Matrix HD cable is a unique technology from Panduit that is used to reduce signal interference in cases of Alien Crosstalk (interference between multiple cables in a bundle) and Electromagnetic Interference (interference from electromagnetic waves).
The concept of Vari-MaTriX is to use a metal tape to wrap around all four pairs of the copper wires in the cable. The tape used for this wrapping consists of multiple pieces, each with different lengths, to create physical properties that can reduce signal interference.
This technology plays a crucial role in enabling the Panduit Cat6A Vari-Matrix HD cable to meet the standards set for Cat6A cables, and also reduces cable size compared to previous technologies. This is because the technology uses less space within the cable itself, and thus the main reason why the Panduit Cat6A Vari-Matrix HD is now the smallest 23 AWG UTP cable in the world.
- Supports Power over Ethernet (PoE++) through UTP cable.
The Panduit Cat6A Vari-Matrix HD cable is designed to support both PoE (IEEE 802.3af), PoE+ (IEEE 802.3at), and PoE++ (IEEE 802.3bt Type 3 and Type 4) standards and can operate in high-temperature environments up to 75 degrees Celsius. This allows it to fully withstand the heat generated from PoE power delivery in each of the above standards.
Furthermore, due to the smaller size of the cable, the Panduit Cat6A Vari-Matrix HD cable can better dissipate the heat generated from using PoE. This helps to reduce the risk of poor signal quality due to lower heat, as well as the risk of fire hazards. Panduit Cat6A Vari-Matrix HD thus enhances the cabling system design in modern buildings, where a large number of Cat 6A cables need to be installed to various points throughout the building to support high network traffic and IoT devices powered through PoE.
- Safety is improved using Low Smoke Zero Halogen (LSZH) fire rating.
The Panduit Cat6A Vari-Matrix HD cable employs Low Smoke Zero Halogen (LSZH) material in its cable jacket, just like other high-quality Panduit cables. LSZH is a material made up of thermoplastic or thermoset compounds, which is utilized here for the cable jackets. When exposed to high heat, LSZH material produce less smoke and release zero toxidity as it does not contain halogen chemical. This significantly enhances safety during a fire incident, thereby allowing building occupants to evacuate safely and facilitating the work of firefighters.
- Environmentally friendly due to its compact design.
As the Panduit Cat6A Vari-Matrix HD cable is the world’s smallest cable produced, it uses fewer materials in cable production. Concurrently, small-sized equipment for Cat6 can also be used in some projects, allowing for the continued use of existing systems or the ability to run multiple lines with fewer devices needed for the overall project.
Another noteworthy feature of the Panduit Cat6A Vari-Matrix HD cable is its support for 1-10GbE speeds in accordance with Cat6A standards, as well as PoE++. This means that the cable can accommodate current and future technologies for many years to come, without the need for cable replacement to meet the requirements of devices demanding higher speeds or electrical power in the future.
Ideal applications for the Panduit TX6A cable
The versatility of the Panduit Cat6A Vari-Matrix HD enables it to be used effectively in numerous applications, such as:-
- The ability to support the latest Wireless Access Points, including WiFi 6E and WiFi 7. This enables it to provide high-speed connectivity while also facilitating power delivery through PoE++.
- When setting up a Digital Building, there's often a requirement for numerous cables runs to cater for multiple applications. By utilizing the Panduit Cat6A Vari-Matrix HD, which has a smaller size, the cost of cable runs can be significantly reduced. Furthermore, it delivers high-speed connectivity and supports PoE++ for a range of devices.
- PoE++ is crucial for several projects that demand PoE/PoE+/PoE++ power delivery to network and IoT devices. Besides supporting these standards, the compact size of Panduit Cat6A Vari-Matrix HD cable improves heat dissipation, reducing the likelihood of signal degradation or fire hazards.
- 5G Distributed Antenna System (DAS) requires high connection speeds and excellent signal interference protection. In this regard, the Panduit Cat6A Vari-Matrix HD is a well-suited option.
In conclusion, the Panduit Cat6A Vari-Matrix HD offers businesses new possibilities with its superior Cat6A UTP cable technology. If an organization aims to invest in a Cat6A cable system for long-term, sustainable business practices, consider using the Panduit Cat6A Vari-Matrix HD as a viable option for designing their in-building cable system without delay.