— Published on 12 Aug 2024

Cable cleats are often overlooked components in electrical installations, yet they play a crucial role in ensuring safety and reliability. In this blog post, we'll delve into the importance of cable cleats, the standards in APAC, the different types of cable cleats and how to select the right ones.
Cable cleats are vital components in electrical installations, providing crucial support and protection for cables. They prevent excessive movement, especially during short circuits or faults, maintaining cable integrity and reducing the risk of damage or hazards.

In the APAC region, adherence to standards ensure the quality, safety, and regulatory compliance of cable cleats. Notable standards include International Electrotechnical Commission (IEC) 61914, national standards such as AS/NZS 2053 (Australia), IS 13947 (India), GB/T 29530 (China), and JIS C 5419 (Japan), as well as industry-specific standards like DNV, ABS, API, and UL Standard 62275.

Various types of cable cleat cater to different cable configurations and installation requirements. These include single cable cleats for securing individual single-core and multicore power cables, trefoil cable cleats specifically engineered for single-core power cables in trefoil arrangement, and multi-cable cleats designed for bundling multiple single-core cables together, such as in Quad arrangement, to maintain balanced loading and reduce electromagnetic interference. Innovative solutions like Panduit Locking and Buckle Strap Cleats offer faster installation, up to 2x faster than conventional cable cleats, with a 50% reduction in material cost, and flexibility for multiple cable or cable ladder configurations. View how easy the installation of Panduit Strap Cleats can be!

Selecting the right cable cleats involve considering cable diameter, short-circuit ratings, environmental conditions, and installation methods. Cable diameter must be matched to cleat size, short-circuit ratings should ensure the cleats can withstand fault forces, environmental factors such as temperature and moisture should be accounted for, and the appropriate installation method—whether on walls, cable trays, or other structures—must be determined.
In conclusion, cable cleats might be small components, but their impact on electrical safety and reliability is significant. Understanding their importance, selecting the appropriate type, and ensuring compliance with relevant standards mitigate risks and ensure optimal performance in electrical installations across the Asia-Pacific region.
References:
Large Paragraph Text Used As A Subheading
Pellentesque non magna eget ex lobortis finibus. Lorem ipsum dolor sit amet, consectetur adipiscing elit. Etiam nec arcu non eros hendrerit viverra a vitae libero. Etiam et ultricies nulla. Donec euismod lectus magna, eu dignissim mauris hendrerit vulputate.
| Time | Place | Details |
|---|---|---|
| 10:00 am - 10:55 am | Expo Hall | Meet and greet in the lobby outside the Expo Hall before the General Assembly. |
| 11:00 am - 11:55 am | Rm 314 | Expert Track: TOP 10 WAYS TO MAKE A DIFFERENCE IN THE INDUSTRY | John Dough, CFO Marketizingly |
| 11:00 am - 11:55 am | Rm 159 | Social Track: MODERN NETWORKING | Hosted by: SponsorName |
Pellentesque non magna eget ex lobortis finibus. Lorem ipsum dolor sit amet, consectetur adipiscing elit. Etiam nec arcu non eros hendrerit viverra a vitae libero. Etiam et ultricies nulla. Donec euismod lectus magna, eu dignissim mauris hendrerit vulputate.