FlexFusion™ Cabinets offer a unique universal platform for all types of data centers and servicing needs including Hyperscale, Edge and Multi-Tenant Data Center. Built with best-in-class weight load of 3,500 lbs. and doors with maximum air flow of 80%, FlexFusion can tackle your most challenging cabinet installations. Whether it’s for server, network or hybrid applications, FlexFusion Cabinets deliver performance to keep your networks running at optimal efficiency.
Additional FlexFusion™ features include:
We have expanded our cabinet series to include FlexFusion XGL Cabinets. These are the preferred choice for applications that require maximum flexibility in data center, enterprise or colocations deployment. Select from the 16 pre-configured models that are equipped with the essential options that provides a simple cost-effective cabinet solution.
FlexFusion XGL Cabinet benefits:



We have performed various testing to assure that Pan-Steel Stainless Steel Cable Ties outperform its competitors in tensile strength, reliability and low thread force. Stainless Steel cable ties are the industry’s standard in harsh environment bundling applications where installation needs to be fast and reliable. The locking ball mechanism locks the tie in place once the body is threaded through the head, creating a secure lock. Panduit has tested our metal locking ties to prove our design superiority and performance.
For more information on Pan-Steel Stainless Steel Solutions, visit our landing page here: Stainless Steel Cable Ties & Cable Management - Panduit.
Or take a look at our Pan-Steel Stainless Steel Cable Ties-Competitive Testing Flyer

It is very important for everyone's safety to make sure that the power is off before opening an electrical device or cabinet and starting work.
But how can one be sure that the circuit is de-energized?
What if, the only acceptable method is a complex testing procedure that may expose the worker and others to the very hazard that needs to be avoided? Panduit has the right solution with VeriSafe 2.0 - an absence of voltage tester (AVT) - that lets you prove the circuit is de-energized.
Learn more about our new voltage-free testing solution.
Go to the VeriSafe 2.0 Landing Page.

The trades of modern building technology are merging under the umbrella of automation. This also applies to professional audio-video (AV) solutions, such as those used in conference and meeting rooms. Here, too, the trend towards increasingly efficient building utilization plays a role. In this article, you can learn about the product solutions Atlona can offer to help you create a smart and efficient building.
Read the article here